The Raritan Blog

Worldwide Data Center Predictions 2018 and Beyond: Part 1

Jessica Ciesla
June 19, 2018

The IT world has reached a bit of a conundrum. The rate at which technological advances are being achieved is starting to outpace data center capabilities. Namely, data centers are working overtime to balance three main workload priorities: rapid resource delivery, control, and low latency. In order to maintain a state of continuous innovation and process improvements, data centers must not only balance these workload priorities, but they must also account for other factors that are driving new ways of thinking.

What Factors Are Driving Data Center Changes?

Data centers are constantly evolving to best meet the needs of the businesses that they serve. As such, there are a few notable factors that will greatly influence the future of data centers. 

•    Pace of Change. -- Data centers need to have technology solutions that are agile and capable of meeting the rapid changes of speed that digital businesses often experience. 
•    Innovation Impasse. -- Once again, legacy systems continue to offer innovative issues. Legacy systems have historically constrained transformation; as such, this challenge will need to be overcome as migrations are completed.
•    Autonomous Infrastructure. -- Experts predict that large data centers will make autonomous infrastructure a standard component.
•    Shifting Economics. -- The rise in digital capital poses a potential change to value structures. Time will tell just how large of an impact digital capital will have on the industry.
With the above factors in mind, as well as the continuous need to balance rapid resource delivery, control, and low latency, experts predict that data centers will experience the following changes within the next few years. 

Prediction #1: Agility, Manageability, and Enhanced Asset Usage Will Drive Digital Transformation. 
It is predicted that by the end of 2019, over 50 percent of IT infrastructure in both data centers and edge locations will be migrated to a software-defined model. This migration will be a direct response to the need for improved agility, enhanced asset usage, and the desired elimination of management silos.

What will be the impact of this change? 

•    Businesses will need to cultivate the in-house or outsourced skills needed to complete automation and asset reclamation tasks. 
•    An increased speed to market mentality will be embraced. 
•    Cooperation across silos will become a priority as more responsive approval systems are adopted.
•    Faster adoption of advanced applications at data centers.

A potential shortage of the right skills and restructuring teams will be the main challenge of the predicted migration to a software-defined model, in both data centers and edge locations. 

Prediction #2: 55 Percent of Enterprises Will Modernize Their Data Center Assets By 2020
It is no secret that the next generation of applications and IT architectures requires heavy workload demands. As a response to these demands, it is predicted that by 2020, 55 percent of enterprises will modernize their data center assets.

What will be the impact of this change? 

•    Businesses will need to invest in smarter DC technologies.
•    Changing data sovereignty and privacy laws will need to be carefully considered and responded to (especially as they affect DC placement).
•    Data centers will need to be carefully analyzed for their cost, performance, and risk factors.
•    Many IT processes will be streamlined as automation is embraced.

An elevated role in both data security and governance practices will need to be addressed as data center assets are modernized to meet the new workload demands.

The Bottom Line: Change Can Only Be Embraced If the Right Skills Are Present
As data centers continue to change, it is important that the skills of in-house and outsourced teams are carefully assessed. After all, the ability to assess agility, manageability and enhanced asset usage is only possible with certain IT skills. Additionally, responding to the need for modernized data centers requires the ability to carefully consider the benefits and limitations of traditional, converged, and software-defined models. As we will see in Part 2 of this series, IT skills will play a significant role as technological innovations, business needs, and workload demands shape the future of data centers.

To learn more, read Part 2 of this series. 

###

Sources:

  • IDC FutureScape: Worldwide Datacenter 2018 Predictions

Other Blog Posts

Universal Input: Delivering Seamless Plug-and-Play Flexibility in Data Centers with Universal Input
Posted on January 12, 2026
The Intelligent PDU: A Critical Component for Power Management in AI Data Centers
Posted on December 17, 2025
How Remote Medical Scanning Streamlines Operations and Improves Patient Satisfaction
Posted on November 24, 2025
Why Residual Current Monitoring Is Essential in Data Centers
Posted on November 24, 2025
Optimizing Data Center Rack Resiliency for AI Workloads
Posted on November 24, 2025

View all Blog Posts

Subscribe


Upcoming Events

CiscoLive 2026
May 31 – June 3  •  Mandalay Bay Convention Center - Las Vegas, NV
2026 OCP Global Summit
October 12 - 15  •  San Jose Convention Center - San Jose, CA
DCD Connect VA
November 3 – 4  •  Lansdown Resort - Leesburg, VA
Dell Technologies World
May 18 - 21  •  The Venetian - Las Vegas, NV

View all Events

Latest Raritan News

Greater Choice, Scalability, Speed: Why Legrand is Doubling Down on Open Compute Project Innovations
Posted on October 3, 2025
Legrand Brings Greater Flexibility to Data Center Operators with New Intelligent Rack PDU Universal Input Option
Posted on February 26, 2025
Legrand Expands Full Suite of DX2 SmartSensors, Keeping Data Centers Ahead of Rack Power and Environmental Monitoring Challenges
Posted on December 18, 2024
Legrand Wins Back-to-Back Awards for Intelligent Rack Power Distribution Innovation
Posted on May 24, 2024
Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications
Posted on April 1, 2024

View all news