The Raritan Blog

Engineering Rack-Level Infrastructure for High-Performance Environments
How HPC and AI Workloads Are Reshaping Rack Design

July 28, 2026

High-performance computing environments are evolving rapidly. As AI adoption accelerates and compute density rises, the rack is becoming a critical point of infrastructure design. Delivering more power into a smaller footprint is no longer enough—operators must also balance safety, flexibility, cooling, and long-term scalability.

Traditional rack-level power architectures were designed for predictable workloads and moderate densities. Today’s HPC environments require a different approach. GPU-heavy applications, open compute deployments, and emerging high-voltage power strategies are pushing infrastructure far beyond historical norms.

Rising Density Is Changing Rack Design

Power densities that once fit comfortably within traditional distribution models are increasing quickly. Standard 60A and 400V architectures are giving way to higher-capacity approaches, with 100A and 125A distribution becoming more common in high-density deployments.

As power demand increases, operators are finding that the capacity of a single PDU is no longer sufficient. Multiple PDUs, stacked power shelves, and higher-current busbars are becoming part of the rack architecture itself.

This shift changes how infrastructure is planned. Rack-level power can no longer be treated as a supporting component—it must be engineered as an integrated system built for density, reliability, and growth.

The Growing Influence of Open Compute

Open Compute architectures are increasingly important in high-performance environments. Designs such as The Open Compute Project’s ORv3 standard reduce cabling complexity while increasing flexibility in power distribution and component placement.

For operators pursuing higher-density environments, open compute power shelves provide a practical path to scaling. Multiple shelves can be stacked to support increasing power requirements while improving rack efficiency.

At the same time, these architectures introduce new considerations around physical integration. Vertical busbars, power shelves, cooling components, and monitoring systems must coexist within increasingly constrained rack footprints.

Planning for AC, DC, and What Comes Next

As rack densities climb, operators are also evaluating the future of power distribution. Traditional AC remains familiar and widely adopted, but higher-voltage DC architectures are gaining attention as a way to support extreme density while reducing current loads.

Some organizations have deployed ±400VDC environments, while others are evaluating 800VDC approaches. These decisions are often influenced by workload type, facility design, and long-term scalability goals.

The transition will not happen all at once. Many environments will support hybrid architectures for years, combining familiar power strategies with emerging technologies as infrastructure evolves.

Physical Integration Matters

Higher-density racks create new physical challenges beyond power delivery. Larger busbars, additional PDUs, and expanded cooling systems compete for limited space inside the cabinet.

As a result, infrastructure design becomes an exercise in integration. Cabinet selection, airflow strategy, cable routing, and power placement must all be coordinated to ensure performance and serviceability. Successful deployments increasingly rely on solutions planned, tested, and validated as a complete system rather than assembled as separate components.

Designing for Flexibility

The pace of change in HPC environments means operators must design for what comes next—not just what exists today. Hardware supporting AI, supercomputing, and HPC workloads continues to evolve, and power requirements are expected to keep climbing. Modular infrastructure, adaptable rack designs, and scalable power architectures help reduce long-term risk while enabling future deployments.

For many operators, the goal is not simply to prepare for higher density, but to build infrastructure that can evolve alongside changing workloads and technologies.

Looking Ahead

High-performance environments are reshaping expectations around rack-level infrastructure. Power delivery, cooling integration, and monitoring must work together to support increasingly dense compute environments.

As AI and HPC continue to drive change, infrastructure strategies will need to evolve alongside them. The racks of tomorrow will not simply hold equipment—they will become engineered systems designed to support performance, resilience, and scale.

To learn more about how rack-level power, open compute infrastructure, and integrated system design are evolving for high-performance environments, explore Legrand’s portfolio of Open Compute cabinets, vertical busbars, and power solutions.