The Raritan Blog

Secure by Design: What to Look for in a Modern KVM Platform
Why Security Architecture Matters for Out-of-Band Management

July 28, 2026

For years, remote access technologies were evaluated primarily on functionality. The ability to connect to a system, diagnose an issue, and restore service quickly was often the primary consideration when selecting a management platform. Today, that conversation is changing. As cyber threats continue to evolve, infrastructure teams are placing greater emphasis on how remote management platforms are engineered—not simply what they can do.

Recent vulnerabilities discovered in several IP KVM platforms have reinforced that shift. While the specific flaws affected only certain products, they served as a reminder that management infrastructure represents one of the most privileged access paths into the data center. As a result, organizations are looking beyond basic functionality and evaluating whether remote access solutions are built on a secure foundation.

Management Infrastructure Has Become Part of the Security Perimeter

As endpoint protection has become more sophisticated, attackers have increasingly turned their attention to management interfaces that operate outside the operating system. Technologies that provide BIOS-level or firmware-level access offer tremendous operational value, but they also require a higher standard of protection because they operate beyond the reach of many traditional security controls.

This evolution has changed expectations for infrastructure teams. Selecting a KVM platform is no longer simply an operational decision—it has become part of a broader cybersecurity strategy focused on protecting privileged access throughout the infrastructure lifecycle.

Security Starts Before You Log In

Modern platform security begins long before an administrator enters a username and password. It starts with establishing trust at the hardware and firmware level, ensuring the platform itself has not been altered before it is ever placed into service.

Features such as Secure Boot, Trusted Platform Module (TPM) support, digitally signed firmware, and trusted cryptographic libraries help create that foundation. Together, these technologies establish a chain of trust from system startup through ongoing operation, reducing the risk of unauthorized software or firmware compromising the management platform.

Strong authentication, encrypted communications, and role-based access controls remain essential, but they are most effective when layered on top of a platform that was designed with security at its core.

Evaluating Secure Remote Access

Organizations today have several options for remotely managing critical infrastructure, each with its own operational and security considerations.

Embedded Baseboard Management Controllers (BMCs), many of which rely on IPMI, provide valuable management capabilities but have historically required careful hardening to address well-documented security concerns. Likewise, software-based remote desktop solutions depend on agents running inside the operating system, potentially expanding the attack surface while limiting access if the operating system becomes unavailable.

Out-of-band KVM platforms take a different approach by operating independently of the host operating system. This allows administrators to maintain secure access during system failures while reducing reliance on software agents installed on production servers.

When evaluating any remote management solution, organizations should look for capabilities such as:

  • Secure Boot, TPM support, and digitally signed firmware
  • Strong authentication with role-based access controls
  • Modern cryptographic libraries and encrypted communications
  • Secure firmware update processes
  • Comprehensive logging and audit capabilities

Security by Design

These architectural principles are reflected in enterprise-grade KVM platforms such as Raritan Dominion KX. Rather than treating security as a collection of individual features, the platform incorporates Secure Boot, TPM support, trusted cryptographic libraries, strong authentication, role-based permissions, secure firmware management, and detailed audit logging as part of a broader secure-by-design philosophy.

This layered approach helps organizations protect privileged access while supporting the operational flexibility required in today’s distributed data center environments.

Looking Ahead

As infrastructure continues to evolve, remote management platforms will play an increasingly important role in both operations and cybersecurity. The organizations best prepared for that future will be those that evaluate KVM platforms not only by the features they offer, but by the security architecture that underpins them.

Security is no longer something added after deployment. Increasingly, it begins with selecting infrastructure that was designed to protect privileged access from the moment it powers on.

To learn more about how Raritan’s secure-by-design KVM-over-IP solutions help organizations protect critical infrastructure, explore the complete Dominion KX portfolio.