The Raritan Blog

The Top 3 Features of Enterprise KVM-Over-IP

Michael Bord
June 3, 2014

Cloud Datacenter KVM-over-IP

Companies with hundreds, if not thousands of servers need an effective and secure way to manage them all remotely. Despite the popularity of software based remote access tools and embedded services over the past decade, neither provides the same level of performance and security as a KVM switch. It’s one of the reasons top government agencies and leading financial institutions still rely on KVM-over-IP.  These are the top three features of enterprise KVM-over-IP that make it the superior remote access tool.

1.  They Feature BIOS-Level Remote Access

In a perfect world, your servers would never get hung up or crash. But alas this all too common reality is enough to frustrate both business users and the IT staff that must hustle to restore critical services! While software based tools require a running OS, and embedded services require an additional port, only KVM provides true out-of-band remote access that allows you to reboot remotely.

2. They Provide At-the-Rack Performance

A true enterprise KVM switch can provide blazing fast video and audio that’s just as good as working on the rack directly.  This allows IT staff to perform server maintenance and troubleshooting in less time and helps to avoid a great deal of frustration that may arise when working with a slower KVM that only provides access with a great deal of lag!

3. They Do Not Compromise on Security

Software based remote server management systems have well documented security flaws; some studies assert that poorly configured software access tools are responsible for 62% of breaches. Embedded service processors were recently revealed to have shocking vulnerabilities such as the ability to login without authentication and the use of cleartext to store passwords. Enterprise KVM on the other hand features government mandated protocols like: AES & FIPS 140-2 encryption, Common Access Card (CAC) authentication, and IPv6 networking.

When you take these three features into account with the fact that many enterprise KVM switches can accommodate up to 8 users working on up to 64 servers, support BIOS-level access over mobile devices, and even virtual media over IP for remote installation, booting, and diagnostics – it becomes clear that choosing an enterprise KVM for remote access isn’t one of several options, it’s the only one.

Test drive the Dominion® KX III Enterprise KVM-over-IP switch from your computer right now to see how you can improve your remote server management capabilities! 

Other Blog Posts

Engineering Rack-Level Infrastructure for High-Performance Environments
How HPC and AI Workloads Are Reshaping Rack Design
Posted on July 28, 2026
Secure by Design: What to Look for in a Modern KVM Platform
Why Security Architecture Matters for Out-of-Band Management
Posted on July 28, 2026
How AI and NVIDIA MGX™ Are Changing Rack Design for Hyperscale and Neocloud Environments
Posted on July 13, 2026
Understanding Neocloud Infrastructure in the Age of AI
Posted on June 1, 2026
Beyond Containment: How Advanced Sensing Is Changing Data Center Cooling
Posted on June 1, 2026

View all Blog Posts

Subscribe


Upcoming Events

2026 OCP Global Summit
October 12 - 15  •  San Jose Convention Center - San Jose, CA
DCD Connect VA
November 3 – 4  •  Lansdown Resort - Leesburg, VA

View all Events

Latest Raritan News

Legrand Introduces Next-Generation KVM Platform Built to Bring Critical Systems Back Online in Minutes
Posted on July 20, 2026
Greater Choice, Scalability, Speed: Why Legrand is Doubling Down on Open Compute Project Innovations
Posted on October 3, 2025
Legrand Brings Greater Flexibility to Data Center Operators with New Intelligent Rack PDU Universal Input Option
Posted on February 26, 2025
Legrand Expands Full Suite of DX2 SmartSensors, Keeping Data Centers Ahead of Rack Power and Environmental Monitoring Challenges
Posted on December 18, 2024
Legrand Wins Back-to-Back Awards for Intelligent Rack Power Distribution Innovation
Posted on May 24, 2024

View all news