The Raritan Blog

Secure Switches Can Defend Against Cyber Attacks

Jessica Ciesla
May 29, 2018

The threat of cyber-attacks seems to reach a new all-time high daily, as cyber criminals continue to become better funded and more sophisticated in their efforts. In fact, a recent PWC report showed that the number of security incidents across all major industries rose by an unprecedented 38 percent. Conversely, data theft from utility companies tripled from 2014 to 2015 by an astonishing 234 percent. In light of these statistics and the rising number of attacks, many companies are left searching for a solution that will protect their vital data and defend against cyber-attacks.

A Simple, Yet Powerful Solution

Secure KVM (keyboard, video, and mouse) switches are a simple, yet powerful solution used to protect vital data from cyber criminals. These switches have been effectively used throughout government, military, and utility networks for years. In fact, they are specifically designed to enhance operator efficiency by eliminating the need for multiple keyboard and mouse systems, as well as effectively removing the possibility of sharing data between multiple systems and networks. In short, Secure KVM switches provide a win-win solution that can help to defend against cyber-attacks by isolating systems and their data.

Leverage a Powerful Cybersecurity Tool

Not only can KVM switches defend against cyber-attacks, but they also offer an added ROI through the following advantages:

• Air Gap Defenses. -- Secure KVM switches can and should be used to maintain heightened cybersecurity measures. They are able to segregate and isolate cyber assets through an “air gap” defense, by isolating the different servers connected to the switch.  This can help to thwart signaling attacks and prevent data leakage.   
• Isolating USB Ports. -- Secure KVM switches can be used to increase security by isolating exposed USB ports. Through this innovative technology, attempts to use USB flash drives or other USP peripherals that might accidentally expose the server to malware can be effectively stopped. Additionally, the audio output inside of the KVM can be set to prevent cyber attackers from using a built-in microphone to launch a signaling attack.
• Meeting Cybersecurity Standards. -- As seen through their successful use within military, government, and utility networks, KVM switches are designed to meet rigorous cybersecurity standards. They are tested, audited, and certified by the NIAP to ensure a heightened level of protection on both classified networks and systems. Finally, they can be used in conjunction with biometric readers to help companies successfully deploy a multi-factor authentication solution. 

The moral of the story is simple, KVM switches can and will effectively help to disable cyber-attacks. By blocking signals, eliminating unnecessary and risky data sharing, providing additional control, and removing desktop clutter, KVM switches are an effective tool that should be used to combat the growing number of cyber threats and attacks. This powerful technology not only increases user productivity and efficiency but also effectively defends against cyber-attacks and limits their destructive power. 

For more information on how Raritan's KVM switches can prevent future cyber-attacks, click here.
 

Other Blog Posts

Understanding Neocloud Infrastructure in the Age of AI
Posted on June 1, 2026
Beyond Containment: How Advanced Sensing Is Changing Data Center Cooling
Posted on June 1, 2026
Universal Input: Delivering Seamless Plug-and-Play Flexibility in Data Centers with Universal Input
Posted on January 12, 2026
The Intelligent PDU: A Critical Component for Power Management in AI Data Centers
Posted on December 17, 2025
How Remote Medical Scanning Streamlines Operations and Improves Patient Satisfaction
Posted on November 24, 2025

View all Blog Posts

Subscribe


Upcoming Events

2026 OCP Global Summit
October 12 - 15  •  San Jose Convention Center - San Jose, CA
DCD Connect VA
November 3 – 4  •  Lansdown Resort - Leesburg, VA

View all Events

Latest Raritan News

Greater Choice, Scalability, Speed: Why Legrand is Doubling Down on Open Compute Project Innovations
Posted on October 3, 2025
Legrand Brings Greater Flexibility to Data Center Operators with New Intelligent Rack PDU Universal Input Option
Posted on February 26, 2025
Legrand Expands Full Suite of DX2 SmartSensors, Keeping Data Centers Ahead of Rack Power and Environmental Monitoring Challenges
Posted on December 18, 2024
Legrand Wins Back-to-Back Awards for Intelligent Rack Power Distribution Innovation
Posted on May 24, 2024
Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications
Posted on April 1, 2024

View all news