Home » Raritan Blog » Raritan PX4 Rack PDUs Pass Rigorous VAPT Security Testing
April 17, 2025

Data centers are increasingly targeted by cybercriminals aiming to steal sensitive information or cause major disruptions to critical systems. A recent PwC report highlights this alarming trend: the number of large-scale breaches is climbing, with 36% of companies reporting incidents costing over $1 million, up from 27% the previous year.
To defend against these growing threats, every component of a data center’s infrastructure must be designed with cybersecurity in mind.
As part of our commitment to provide the most secure and reliable rack power distribution products, we put our PX4 Rack PDUs through an independent third-party review for vulnerability and penetration testing. We partnered with CBIZ Pivot Point Security (CPPS), a third-party testing company known for its ability to challenge and determine if technology products meet industry best practices for digital security.
The Test
We partnered with CBIZ Pivot Point Security (CPPS) to conduct an IoT security assessment and Vulnerability and Penetration Testing (VAPT) on our PX4 Rack PDU and its embedded firmware. While our testing and quality teams strive to follow the industry’s best practices, review current vulnerability notices, and with other third-party tools, conduct our own vulnerability testing, we wanted to ensure that we're identifying and mitigating security risks and uncovering hidden weaknesses that may have been overlooked.
As part of this initiative, we also asked CPPS to verify our compliance with California SB-327. This regulation requires reasonable security features should be available to protect devices from unauthorized access, destruction, use, modification, or disclosure. Our compliance requires users to, after the first product login, change the default password to ensure ongoing security once a device is installed.
In addition, we specifically wanted CPPS to report on whether our products’ security measures were consistent with industry best practices outlined in the National Institute of Standards and Technology Interagency Reports (NISTIR) 8259. NISTIR 8259 is the second edition of NIST’s standard, “Foundational Cybersecurity Activities for IoT Device Manufacturers.” NISTIR 8259 recommends cybersecurity activities that manufacturers should perform before they sell their IoT devices to customers.
The Results
Following a broad scope of testing that covered device firmware, SDKs and APIs, cryptographic keys and digital certificates, device-to-device communications such as PDU linking and cascading, port security on the controller, and more, CPPS’ VAPT testing confirmed that the PX4 PDU is secured to a level that is consistent with both industry best practices and par with other tested peer devices.
The CPPS tests validate our ongoing dedication to security throughout the engineering process of our rack PDU products. The full line of PX4 intelligent PDUs features the latest network security protocols, and the most diverse user authentication and management options, leveraging best-in-class data encryption methods.
One of the most valuable aspects of third-party cybersecurity testing is the actionable insight it provides. CPPS not only confirmed the strength of our existing security protocols but delivered recommendations for further hardening our devices (which we implemented!) as well as resolve any issues that may have been identified during the testing process. Our intelligent PDUs are continuously updated to ensure safety during deployment and meet the increased network security requirements in high-risk environments.
To further prove this point, our PDUs employ these security measures to protect our customers’ equipment, data, and networks:
With cybercrime on the rise and new threats constantly emerging, managing cyber risks can seem complicated. Our VAPT testing results have helped us prove our commitment to security and organizational technical controls. Raritan is one of the only PDU manufacturers participating in this type of third-party independent testing.
We have taken this additional time-consuming and expensive testing step to ensure our teams are risk-aware and continue to proactively identify and address weaknesses that may arise in our products. Other key initiatives include our recent ISO/IEC 27001 certification and government approval of USGv6-r1 capabilities—covering Core, SLAAC, Address Architecture, and IPv6-Only—validated through rigorous testing by the University of New Hampshire InterOperability Laboratory (UNH-IOL).
If you would like to learn more about our VAPT testing results or the features available to ensure the security of our PDUs, please contact us.