The Raritan Blog

How AI and NVIDIA MGX™ Are Changing Rack Design for Hyperscale and Neocloud Environments

July 13, 2026

Artificial intelligence is driving a fundamental shift in how data center infrastructure is designed, particularly at the rack level.

As hyperscalers and neocloud providers deploy increasingly dense, GPU-driven workloads, traditional assumptions around rack design are being challenged. While Open Compute Project (OCP) standards have helped establish consistency and efficiency across deployments, real-world implementations are revealing the need for greater flexibility. For operators supporting AI infrastructure, the question is no longer whether to adopt OCP—but how to adapt it.

Why OCP Standards Are Only Part of the Solution

OCP has played a critical role in standardizing rack design, improving interoperability, and accelerating deployment at scale. However, as AI workloads evolve, so do the physical and operational demands placed on infrastructure. GPU-based systems introduce higher power densities, unique thermal profiles, and increased weight loads. At the same time, equipment manufacturers continue to innovate, often requiring configurations that extend beyond standard rack dimensions and mounting approaches. As a result, even in highly standardized environments, customization remains essential.

What’s Changing at the Rack Level for AI Deployments

As hyperscale and neocloud environments evolve, several key shifts are taking place at the rack level:

  • Increased power density driven by GPU-intensive workloads
  • Greater demand for integrated cooling strategies
  • Non-standard cabinet widths and depths to support specialized equipment
  • More complex cable management requirements
  • The continued use of EIA/ECA-310 (19-inch) mounting alongside OCP structures

These changes reflect a broader trend: infrastructure must now accommodate both standardization and variation simultaneously.

How Legrand’s MGX/NVL Cabinet Addresses These Challenges

Legrand’s MGX/NVL cabinet is designed to support the latest AI infrastructure requirements while maintaining alignment with OCP principles. By combining standardized design with targeted customization, the platform enables operators to meet evolving demands without sacrificing consistency. One of the most significant advantages is the cabinet’s integrated frame construction. By incorporating MGX cooling capabilities directly into the cabinet design, operators can reduce the need for additional components and minimize on-site installation complexity.

Customization is another critical factor. The MGX/NVL cabinet supports flexible widths and depths, allowing operators to accommodate non-standard equipment configurations and address increasingly complex cable management needs. This flexibility is particularly valuable in AI environments, where hardware requirements can vary significantly between deployments. At the same time, the cabinet maintains compatibility with existing infrastructure standards. The ability to mount 19-inch rails within an OCP-based structure—using blanking panels where needed—ensures that operators can support a mix of legacy and next-generation equipment within the same environment.

Flexibility Is Now a Core Requirement

As AI infrastructure continues to evolve, the ability to adapt quickly at the rack level is becoming a competitive advantage. Operators are no longer designing for a single, fixed configuration. Instead, they must plan for ongoing change—whether that means higher power densities, new cooling approaches, or shifting equipment requirements. Solutions that combine the consistency of OCP standards with the flexibility to support customization will be better positioned to meet these demands.

Looking Ahead

The rise of neocloud and hyperscale AI deployments is redefining what rack infrastructure needs to deliver. While standards like OCP remain essential, they are only part of the equation. To support next-generation workloads, operators need solutions that can bridge the gap between standardization and real-world variability. To learn more about Legrand’s open compute products and how the MGX/NVL cabinet supports AI-driven infrastructure, explore the full portfolio and download the MGX/NVL specification sheet.