Home » Raritan Blog » Disruptive Technologies Changing Data Centers: Part 3
Rick Gonedes
August 14, 2018

Content originally sourced from 451 Research.
Disruptive technologies will have the unique opportunity to positively impact data centers. In Part 2 of this series, we explored two technologies that are staged to change the very system and infrastructure of IT systems. In this final portion of our disruptive technologies series, we want to take a look at two technologies that will bring heightened levels of agility to data centers for a fraction of the cost.

Disruptive Technology #1. Open Source Infrastructure
Reports indicate that some of the largest data center operators have already begun to adopt open architectures meaning deploying technologies that allow easy modification and updates. This adoption is done to not only lower costs but to also glean the benefits of simplification and standardization. With an open source infrastructure, data center operators will be able to realize savings by leveraging a bare-bones IT hardware solution.
Who will adopt this technology?
Why will this technology continue to be adopted?
Open source infrastructure currently represents up to three percent of global data center spend. However, interest is on the rise, which means that data center operators will need to continue to drive down costs as they increase agility. The adoption of open source infrastructure within data centers might be slow, but the potential ramifications will likely be significant.

Disruptive Technology #2. Software-Defined Power
A software-defined data center is where all components including compute, storage, networking, and security—are virtualized, or decoupled from specific physical hardware and software-defined power is based around creating a layer of abstraction that will continuously match power resources with the ever-changing needs of the data center. The reason behind this disruptive technology is two-fold -- 1) to achieve significant cost savings, and 2) to improve the agility of the data center by treating its power as a virtual resource that can be effectively managed.
Who will adopt this technology?
Why will this technology continue to be adopted?
If software-defined power can offer the same availability for mission-critical applications as physical equipment can, then the argument for its adoption is won. Additionally, this disruptive technology offers the clear benefit of lowered costs without adding any additional risk. Finally, if data centers use software-defined power, and other disruptive technologies, to operate at higher utilization levels, then the data centers themselves could in effect become cheaper and smaller.
The Adoption Of Disruptive Technologies Will Continue In Data Centers
One thing is certain, disruptive technologies such as open source infrastructure and software-defined power will continue to be adopted within data centers. As seen with the Chiller free and micro-embedded technologies discussed within Part 1, as well as the Storage-class memory and silicon photonics technologies discussed within Part 2, the world of data centers will continue to evolve as new disruptive technologies enter the marketplace.
###
Sources: