The Raritan Blog

Beyond Containment: How Advanced Sensing Is Changing Data Center Cooling

June 1, 2026

How can data centers improve cooling efficiency without major infrastructure changes? Advanced sensing technologies provide real-time airflow and pressure visibility that helps operators optimize containment performance and sustainability.

When data centers pursue sustainability goals, attention often turns to large-scale investments such as liquid cooling or power infrastructure upgrades. Yet some of the most meaningful efficiency improvements may come from systems already present in the white space—particularly aisle containment.

For years, containment has served a straightforward purpose: separating hot and cold air to improve cooling performance. It has traditionally been viewed as a static component of the environment, designed to manage airflow but not actively contribute to operational insight. As rack densities increase and efficiency expectations rise, that perception is beginning to change.

Moving Beyond Passive Containment

Containment systems have long been treated as infrastructure that simply works in the background. Once deployed, they are rarely measured directly. Operators assume the barrier is functioning as intended, while monitoring efforts remain focused at the cabinet level.

Most thermal monitoring today occurs at the rack, where temperature sensors help ensure equipment remains within acceptable operating conditions. This aligns with common best practices that prioritize protecting high-value IT equipment through inlet temperature visibility.

However, measuring temperature at the rack only tells part of the story. It reveals how equipment is performing but provides limited insight into how effectively airflow is being managed across the containment system itself.

Turning Containment Into a Source of Insight

Advanced sensing introduces a new layer of visibility by measuring what happens within and around containment zones. Rather than treating containment as a fixed boundary, operators can begin evaluating how efficiently air is moving through the environment.

Differential pressure sensing is one example. By comparing pressure inside and outside the aisle, operators can identify whether cool air remains contained or if leakage and recirculation are occurring. Airflow monitoring adds another dimension, confirming whether conditioned air is reaching the intended locations or bypassing equipment entirely.

Together, these measurements help create a clearer understanding of cooling performance. Small inefficiencies that might otherwise go unnoticed—such as uneven airflow distribution or pressure loss—can become visible before they impact uptime or energy consumption.

From Monitoring to Action

Sensor data becomes more valuable when combined with visualization and analytics tools. Modern DCIM and building management platforms can aggregate sensor inputs into dashboards, allowing operators to understand airflow behavior across containment zones in near real time.

This visibility enables practical adjustments that improve efficiency. Teams may fine-tune fan speeds, identify leakage points, or rebalance airflow delivery without relying solely on manual inspections or large-scale modeling exercises.

Compared to computational fluid dynamics studies, sensor-based monitoring offers a factual, real-time means to evaluate containment performance continuously. Plug-and-play sensing strategies can often be integrated into existing monitoring environments without significant disruption or capital investment.

A Smarter Path to Sustainability

As data centers pursue greater efficiency, advanced sensing creates an opportunity to improve systems that have historically remained passive. Rather than relying on assumptions, operators can measure how well containment performs and use that insight to make targeted operational decisions.

Pressure and airflow monitoring will not replace broader cooling strategies, but they can provide a more detailed understanding of how existing infrastructure behaves under real operating conditions. This makes containment more than a physical barrier—it becomes an active contributor to sustainability and performance.

Looking Ahead

Every facility operates differently, and there is no single approach to monitoring containment effectiveness. Some operators may prioritize airflow visibility, while others focus on pressure balance or thermal consistency.

What matters most is gaining a clearer understanding of how cooling systems perform at the aisle level. By pairing advanced sensing with smarter analytics, operators can unlock new opportunities to improve efficiency, reduce waste, and support long-term sustainability goals.

Explore Raritan Smart Sensors and Monitoring Solutions