The Raritan Blog

Why KVM-over-IP Makes Sense for Mac Mini Deployments

Posted on June 30, 2025 by Gento

When Apple introduced the Mac Mini, it was intended as a low-cost desktop option for consumers. In time, the machine found its way into enterprise use, providing a platform to test Apple-specific applications on desktop and mobile devices. However, Apple's proprietary operating system posed some challenges for infrastructure managers.

First, Apple’s closed ecosystem requires programmers to use specific hardware and software beyond the traditional tools used for development and testing. In addition, deploying applications in a scalable, repeatable fashion wasn’t possible because of the tedious process of setting each computer up manually. Each device had to be configured separately, requiring repetitive tasks including installing software and adjusting settings.  

Once set up, each machine had to be added to a mobile device management (MDM) software system for centralized management. It doesn’t take much to realize how time-consuming and labor-intensive all of these steps were. And even after the initial deployment, software management limitations had an impact on the overall lifecycle management of the infrastructure, as it was difficult to update or troubleshoot issues without direct physical access.  

Clearly, infrastructure managers needed a better way to deploy and manage Mac devices. The answer came in the form of KVM (keyboard, video, mouse) technology that lets users control multiple computers from a single terminal.  

Raritan KVM: an Efficient, Scalable Alternative  

After the release of a Mac Mini version powered by Apple’s own silicon in 2020, Raritan received requests from clients for a software development kit (SDK) of our KVM solution. We delivered a client SDK enabling the use of Raritan’s KX III KVM-over-IP switch to automate the deployment of Mac devices. The Dominion KX III lets users manage large fleets of Mac Mini devices remotely and enables direct access to both hardware and software. Tasks that would have otherwise taken hours can now be completed in minutes.  

By leveraging the switch’s KVM capabilities, organizations can create a custom automation program to deploy hundreds or thousands of computers simultaneously. With the KVM client SDK, users can automatically click through all prompts and screens and enter text into the required fields during the initial setup of a consumer-based Mac.

This approach eliminates the cumbersome process of setting up, deploying, and testing each Mac Mini device. It gives infrastructure managers a scalable, repeatable method of deploying macOS computers and performing large-scale testing of applications in a fraction of the time it would take to do these tasks manually.

KVM Boosts Efficiency  

The Mac Mini use case illustrates the value of implementing KVM-over-IP technology to boost efficiency and productivity. Organizations that leverage Raritan KVM products in conjunction with open-source SDKs save valuable time and increase efficiency when testing and maintaining Mac resources.

Raritan’s KVM solutions offer high technical capabilities beyond automating device setup. Infrastructure managers can also leverage them for remote monitoring and maintenance access. This capability not only saves IT managers time, but enables continuous visibility into operating conditions, helping prevent failures. To learn more, access the Mac Mini application overview.  
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
Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications