The Raritan Blog

When Deploying a Centralized IT Management Solution, Leverage the Advantages of a Virtual Appliance

Posted on October 25, 2010 by Website Administrator  |  Comments (2)

Vendors in the IT and data center space are beginning to make their centralized management systems available as a virtual appliance, enabling them to run on leading virtualization platforms. This is the case with Raritan’s CommandCenter Secure Gateway (CC-SG). A new version will be released in November that can be deployed as a VMware virtual machine.

Running as a virtual machine (VM) – especially within a VMware environment that delivers several key features rich in flexibility and security, has several operational advantages over a proprietary hardware solution. For example, there is likely space and resources available in an established virtual environment on which the appliance can be installed. As a result, additional hardware expense is avoided. Also, with a virtual appliance, there is no extended hardware warranty to purchase.