The Raritan Blog

How is the Data Center Optimization Initiative (DCOI) Changing the Landscape? (Part 1)

Posted on May 8, 2017 by Rick Gonedes  |  Comment (0)

Data centers are becoming more important with each passing day. One study estimates that data center construction worldwide will continue to grow at a rate of about 21% per year until 2018. Yet at the same time, the infrastructure that supports these mission-critical data centers is woefully inefficient on their best days. It is estimated that about 30% of servers in the United States alone were considered comatose - meaning that expensive computing assets are going to waste. Worldwide, experts estimate that about 10 million servers (representing about $30 million in capital) have not performed valuable computing work OR delivered data in the past six months.