About Us

Extended IT rack power mapping possibilities with Raritan’s locking solution

Posted on October 23, 2019

Schiedam, the Netherlands (24 October 2019) Raritan, a brand of Legrand, today added two extra colors to its portfolio of popular SecureLock® cables. In addition to black, blue, and red colored cables, customers can now also choose from green and white cables. 

The decision of adding additional colored SecureLock cables was made after data centers increasingly color code their multiple cabinet power distribution chains, thereby requiring an increased number of colors.

The locking cables fitted to SecureLock-ready outlets on intelligent PDUs, such as those from Raritan and Server Technology, prevent mission-critical IT equipment from getting disconnected unwantedly from electricity. The SecureLock solution not only reduces the risk of downtime due to accidental unplugging of cables during data center maintenance tasks or vibration in the rack; it is also a simple but effective way of visualizing power paths in IT infrastructures.

Other than visualizing A and B feeds using two different colors as best-practice datacenter design, there is also an increased requirement to distinguish between the different types of equipment connected to PDUs, visualization of pre-set power paths of different customer configurations (i.e. in co-location facilities), and to easily identify between either different plug types or single and 3-phase connections. Another important application is color coding of multiple UPS power paths, which can be found in data centers looking for extra levels of redundancy.

The CE certified locking cables with a maximum temperature rating of up to 70ºC /158 F. are available in different cable lengths (0.5, 1.0, 1.5, 2.0, 2.5 and 3.0 meter) and different plug types for all kinds of IT equipment including C14/C13, C20/C19, but also C14/C15 connectors with flexible rubber sheeted jackets for high-amperage, high heat devices from vendors such as Cisco®, Dell®, and HP®.

This smart uptime aiding locking solution works both with Raritan PX® intelligent PDUs, transfer switches, and Sever technology PDUs. SecureLock cables come in packs of 6 and are now readily available from stock.

For more information, contact your local Raritan representative, authorized reseller, or Legrand data center specialist teams across EMEA.

# # #

About Raritan
Raritan, a brand of Legrand, is a global leader in intelligent rack PDUs, KVM switches, and other data center infrastructure monitoring and management solutions. Raritan’s innovations improve the reliability, efficiency, and intelligence of data centers and server rooms around the globe — including those of the top Fortune 500 companies, such as Cisco, Dell, Google, HP, IBM, Intel, and Microsoft. To learn more, visit Raritan.com, LinkedIn, or Twitter.

About Legrand
Legrand is the global specialist in electrical and digital building infrastructures. Its comprehensive offering of solutions for commercial, industrial and residential markets makes it a benchmark for customers worldwide. Drawing on an approach that involves all teams and stakeholders, Legrand is pursuing its strategy of profitable and sustainable growth driven by acquisitions and innovation, with a steady flow of new offerings—including Eliot* connected products with enhanced value in use. Legrand reported sales of close to €6 billion in 2018. The company is listed on Euronext Paris and is notably a component stock of the CAC 40 index. (code ISIN FR0010307819) www.legrand.com.

All product and company names herein may be trademarks of their registered owners.

View by Category
Monthly Archives
More Recent News
Legrand Certifications and Process Controls Provide Confidence in Information Security for Network-Connected Devices in Data-Related Applications

—ISO27001 certification delivers assurance to the security of thoroughly tested data, power and control devices from Legrand brands, including the Raritan®, Server Technology® and Starline® brands.

Posted on April 1, 2024
Legrand Releases Version 4.0 of Raritan’s Industry-Leading Secure KVM Switches, Raising Bar for Secure Desktop Access

—Raritan Secure Switches (RSS) meet the stringent requirements of NIAP 4.0 Peripheral Sharing Device and can be implemented to protect government and private sector data.

Posted on July 31, 2023
Legrand Revitalizes Data Center Sector with Two Revolutionary Intelligent Rack PDUs

— Offered by Legrand brands Server Technology and Raritan as the PRO4X and PX4, the new intelligent PDUs offer unparalleled visibility, flexibility, density and security for ever-changing rack power and infrastructure requirements —

Posted on May 1, 2023
Raritan Reveals The MasterConsole® Digital Dual KVM Switch

— New Switch Allows Users to Productively Work With Dual Displays With Borderless Mouse Switching —

Posted on February 18, 2021
Legrand Data, Power and Control Division Announced as Finalist in Six Categories at DCS Awards 2020
Posted on November 9, 2020