主頁 » 部落格
Posted on August 24, 2020 by Gento

雖然三相PDU可提供較高的電力容量,但是需要在部署伺服器之前先進行規劃。PDU三相中的一相或兩相不平衡汲取電力會產生滯留容量,進而增加電力浪費。此外,此情況可能會導致上游出現連鎖故障的情況。PX4 PDU可以主動監控相位之間的平衡,若正確配置,則可在相位不平衡超過特定的閾值時提醒您或您的團隊。作為最佳實務,最重要的是盡可能使全部的三相平衡,以減少意外中斷及電力浪費。
Posted on August 24, 2020 by Gento

Raritan's PX3 PDUs monitor a variety of electrical and environmental parameters. You can receive alerts on anything that gets monitored – inlet data, outlet data, circuit breaker status, unbalanced loads, and power factor, to name a few. To configure and receive alerts successfully, you need to ensure the following actions have been completed:
1. Configure Alert Delivery Mechanism – how to set up and receive your alerts: SNMP and/or SMTP.
a. If you prefer your alerts to be sent to an SNMP manager tool, you need to enable: Device Settings > SNMP > Enable SNMP Notifications
It is important to note that this setting is different from the SNMP Agent setting. You won't be receiving SNMP alerts even if you have enabled SNMP v1/ v2c if you don't explicitly enable SNMP Notifications.
Posted on June 23, 2020 by Gento

The benefits of Network connected KVM switches highlighted in Raritan blog about remote management of IT devices show how businesses can continue as usual while keeping staff safe amidst the ongoing COVID-19 pandemic. Although the worst seems to be over and lockdown restrictions are easing, a resurgence of the infection is still very real. Thus, employees should continue working from home or offsite where feasible, with support from remote tools.
This article gives 8 practical tips when purchasing remote access management solutions to ensure that your business objectives are achieved, while keeping an eye on existing corporate resources to maximize your investment.
Posted on June 15, 2020 by Gento
.jpg)
The COVID-19 pandemic is an evolving world-wide public-health and economic crisis. Companies must keep their business operations and systems running. They also need to keep their employees safe and healthy. Many employees are now working from home, either on a full or part time basis. While the worst seems to be behind us in much of the United States, Europe and Asia, the Center for Disease Control (CDC) is warning that there may be a “second wave” in the fall/winter. Remote management can be of enormous benefit in this type of uncertain environment.
Posted on April 2, 2020 by Gento

Looking for an economical KVM solution? This blog discusses features included in the new Dominion LX II, and why it would be beneficial for you to trade up from the original Dominion LX.
The new Dominion LX II from Raritan is the latest in a line of products designed with the small to midsize business IP KVM switch user in mind. Our new unit is designed to provide economical, Java-free, BIOS-level remote access to between 8 and 16 servers as well as virtual media. The new Dominion also supports connections up to 15 frames-per-second at a resolution up to 1080p and 1200p. With six different options available, the next generation LX II is poised to become the leading SMB IP KVM switch on the market today.