部落格

Benchmark Your Data Center - May 23 in Atlanta

Posted on May 9, 2013 by Gento

Benchmarking your Data Center  

Key Note Speaker: EDI, Ltd.‘s Jeremy Gilbertson, CTS, RCDD  

Topics Covered:
- Why Most Data Center Projects Fail Before They Begin. The importance of benchmarking and accurate statement of requirements
-  State of the Industry – Data Centers: Interesting, unique goings-on in the data center industry  

Jeremy Gilbertson, CTS, RCDD is Vice President of EDI, Ltd.‘s Data Center Practice and is responsible for overall strategic direction, management, and project delivery for the practice. Jeremy’s expertise involves helping enterprise, third-party provider, healthcare, and higher-education clients understand the current state of their data centers and develop phased strategies that address business requirements, risk profile, and budget. 

Join us for an afternoon of leading edge Data Center discussions and real world case studies ranging from design through intelligent infrastructure management followed by a tasting of best brews and appetizers. 

REGISTER HERE
Space is limited.

When:Thursday, May 23rd from 12:00pm-5:00pm
Where: Gordon Biersch Brewery - Buckhead location
3242 Peachtree Road N Atlanta GA 30305
Agenda

Case Studies on Tap:
- Raritan: Deploying High Power at the Rack
- Fluke Networks: Ensuring Performance of Critical, High Bandwidth Fiber Links
- Global Power Technologies: Power Monitoring Systems Enhance the Commissioning Process for a Fully Integrated Facility
- Vigilent Corporation: Too Cool - Changing the Game in Data Center Cooling    

About EDI, Ltd.  EDI, Ltd. is a leading healthcare IT consulting and design firm specializing in medical communication technologies, information systems infrastructure, security, audio-visual systems, and data center.   

Attendees will be entered into a drawing for a Kindle Fire! 

REGISTER HERE
Space is limited.


The Data Center Detectives Discuss PDU Accuracy

Posted on May 8, 2013 by Gento

Accuracy for rack power distribution units (PDU to some, CDU to others) is gaining in importance as energy costs and energy cost management are getting increasing attention. In today’s episode, The Data Center Detectives discuss proper kWh measurement:

sherlock-ohms

Raritan pioneered ISO/IEC 1% accuracy for energy in rack PDU at the outlet level — with first product shipments in the summer of 2008. Today, Raritan has more than 600 models that meet this standard, including custom engineered units.

Don’t miss the next epsiode of The Data Center Detectives — subscribe to our blog.


Visit Us at the Uptime Symposium – Learn and Maybe Even Win

Posted on May 2, 2013 by Gento

Stop by our booth (#219) and see why we were recently named to CRN’s 2013 Data Center 100 list

Get a $600 registration discount on us—Use code RARITANCLIENT Register Now -

Raritan is a proven innovator of power management, DCIM software, KVM and serial solutions for data centers of all sizes. Stop by our booth for live demos to learn about some of our latest solutions, which inlcude:

- SecureLock™ - Never worry about your cables accidentally unplugging
- Wi-Fi Kit - Keep your iPDUs connected with savings, security and easy implementationd
- cTrack - This new release of dcTrack®  3.0 DCIM software provides additional capabilities to make it easier for data center professionals to obtain information on their data center infrastructures

Stop by and be entered into a drawing for an iPad mini.


The Uptime Institutes “State of the Data Center 2013 Survey Results” Confirms DCIM growth

Posted on April 30, 2013 by Gento

The Uptime Institute recently conducted a webinar on the “State of the Data Center 2013 Survey Results.”  Per the survey the adoption of DCIM is expected to continue – and according to the survey, in the next 2 years about 32% of the respondents indicate that they plan to buy.

It was interesting to hear that globally Data Center budgets are expanding and money is being spent to grow their footprint.   In fact in the webinar it was stated that 70% of data center operators built a new site or renovated a site in the past 5 years.  Tools that can provide assistance in the build seem to be essential to success.

Data center operations, deployment and design are capital intensive, so there tends to be a focus on cost and performance by the C-Suite.  In fact the majority of Data Center Managers reported that they provide performance or cost metrics to the C-Suite monthly.   However, depending on the organization size and the tools used, reporting can be complex and/or unavailable.

Through the survey over 80% of the respondents indicated that Facilities generally pays the energy bill, and therefore incurs the cost of inefficiencies.  Finding ways to free up Data Center capacity and reduces costs are top drivers for pursuing efficiency savings.  Additionally, working with IT to implement a solution that supports bill-backs can relieve Facilities of some of the burden.

While cost, integration, and database issues are often significant barriers to deploying a DCIM, the savings that can be received from improved capacity planning and energy efficiency, the ability to identify problems, and the gain in asset visibility make a DCIM solution the most efficient and effective way to manage the Data Center.


In the Data Center Knowledge is (Lower Cost) Power

Posted on April 29, 2013 by Gento

Data-Center-Power-3

In my last post,(link) I described the great volumes of power consumption and environmental data you can get from Raritan’s iPDUs, and how that can help you lower energy costs in the data center. We only scratched the surface, though, of the analytics and reporting capabilities of Power IQ software, and how it enables best practices in power management.

Some of the smarts we’ve put into Power IQ come right from the American Society of Heating, Refrigeration and Air-Conditioning Engineers (ASHRAE). Here, I’m referring to their Psychrometric chart, a guide to optimal temperature and humidity ranges for the data center. You can easily set these parameters to serve as notification thresholds for Raritan’s temperature and humidity probes, or competitors’ probes.

The great news: ASHRAE has recently extended the ranges in that chart, giving you a tolerance that allows you to safely save on energy costs—as noted above, up to 4% for every degree raised.

What’s even cooler (no pun intended)—you can put your own temperature and humidity parameters into Power IQ. That’s useful because many server manufacturers have reengineered their products in recent years to handle harsher environments. Some have even certified their servers to run in 90-to-95-degree environments. You can take those manufacturer’s settings now and incorporate them into your ASHRAE Psychrometric chart. Now you can selectively raise your air temperature and save more on energy.

With the global view of temperatures you get from Power IQ, you can see where you’re over-provisioned or under-provisioned across rows, aisles, and even multiple data centers. You can even see where you’re pumping too much CO2 into the air. Now there’s a feature that’s not only good for your bottom line; it’s the right thing for the environment.

Data Center Energy Provider Rebates

But there’s more: Because Power IQ can actually report on how much CO2 emission has been reduced, that metric yields dollar savings as well. Do a search on “data center energy rebates” and you’ll see that if you can document your CO2 reduction, many energy providers will give you a lower rate.

Being able to say you’ve reduced CO2 emissions by W, KwH by X, power costs by Y, and lowered rates by Z percent makes you a hero in your data center.

Also, Power IQ has joined the great mobile migration. If you want to be not only alerted but empowered to take action if the temperature around a certain server exceeds a certain threshold, there’s a Power IQ app for that. You can get an alert that while you’re away from the data center and proceed to power cycle the affected device, right from your iPhone.

Click here to learn more about Raritan data center power solutions


Page 62 of 68 pages ‹ First  < 60 61 62 63 64 >  Last ›

訂閱

近期活動
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
Raritan最新新聞