主頁 » 部落格
Posted on October 24, 2014 by Gento

What is a KVM Switch?
KVM switches enable users to access and control multiple computer devices from a single keyboard, video and mouse (KVM) console. This includes servers, PCs, workstations and even tablet computers. Anyone requiring access to multiple computing devices over short or long distances can benefit from a KVM switch! This ranges from an engineer switching between multiple computers under his/her desk to an IT administrator maintaining thousands of servers across multiple sites.
Posted on October 21, 2014 by Gento
Couldn't make it to Raritan's booth at AFCOM Orlando this year? Not to worry. See David Wood's presentation on the PX3 -- Raritan's third generation intelligent rack PDU!
Posted on October 16, 2014 by Gento
What is DCIM and why do you need it for your data center? Find out in less than two minutes. See if DCIM is right for your data center.
Posted on October 13, 2014 by Gento

The Power Usage Effectiveness (PUE) metric which was first introduced by The Green Grid™ in 2007 has become the de facto standard for measuring data center efficiency. But despite its prevalence, many data center operators are unclear on what PUE is, how it is calculated, and how it can be used to further energy efficiency initiatives. For instance, many data center managers know that their PUE readings should be as close to the number one as possible, but why?
Posted on October 10, 2014 by Gento

There are some big questions in life and the Institute for Earth Sciences and Astronomy (INSU) aims to answer them. According to its website, priority research areas at INSU mainly cover:
As part of its mission, the INSU utilize an array of sophisticated scientific instruments on Dumont d'Urville Station located in Antarctica on Île des Pétrels, archipelago of Pointe Géologie in Adélie Land. To operate these devices and access the data they amass, researchers rely on Raritan’s Dominion® KX II-101 single port KVM switch for remote access.