主頁 » 部落格
Posted on November 14, 2019 by Gento

As the need for power consumption per server has changed, so too have the outlet density and types of rack PDUs. In fact, in order to support the power-hungry IT equipment that seems to dominate data centers, rack PDUs have become increasingly more powerful. Today's data centers see densely packed racks, greater watts per square foot, and higher than every power consumption. Understanding rack PDUs outlet density and types is a vital to keeping data centers running properly, without overloading servers or creating costly outages.
Posted on September 18, 2019 by Gento

Data centers come in all shapes and sizes. They are built to securely store copious amounts of data. However, what many people don't know is that in order to hold all of the data, these centers must also consume a large amount of energy. In fact, some estimates show that data centers consume 1.8 percent of the total United States energy consumption every year. The large amount of energy that is consumed, as well as other factors, makes environmental monitoring a key component of data center management.
Posted on July 30, 2019 by Gento

Thanks to emerging technologies and increased capabilities, power distribution has become only one component of effectively managing rack PDUs. In fact, rack PDUs are now available with additional capabilities, such as multi-level power metering and power capacity planning, which makes it easier for data center managers to effectively meet established SLAs.
Intelligent PDUs also play a crucial role in eliminating periods of unexpected downtime in the data center. Keep reading to learn more about the true power of an intelligent PDU.
Posted on July 27, 2019 by Gento

To date, the data center industry has had to become innovative as they seek to respond to the increasing demand for power. As part of their innovation best practices, forward thinking data center managers have turned to high-density and high-power rack PDUs with sensors. This technology is designed to help data centers become "green," reduce their carbon footprint, and effectively respond to the ever-increasing demand for power and density of IT equipment at the rack level.
Posted on July 27, 2019 by Gento

Data centers now consume an estimated 1.8 percent of electricity within the United States. As energy consumption has risen, so too have the associated costs. These costs, coupled with the fact that approximately 30 percent of data center servers are either idle or underutilized, have resulted in unnecessary expenses that could have been mitigated with the right environmental monitoring best practices. These best practices include monitoring temperature and humidity in accordance with ASHRAE 90.4.
What Is ASHRAE 90.4 ?
In its simplest forms ASHRAE 90.4 is a new standard that is designed to help data centers effectively monitor temperature and humidity levels so that downtime is reduced, and enhanced efficiencies can be introduced. This standard focuses on the use of on-site and off-site renewable energy. It uses both Mechanical Load (MLC) and Electrical Loss (ELC) to better determine the maximum allowable values for climate zones. At its core, ASHRAE 90.4 helps data center managers understand when they are undercooling their machines and operating at detrimental humidity levels, so that power utilization can be enhanced for the entire data center.