The Raritan Blog

Increase Temperature and Save Energy

Posted on August 2, 2010 by James Cerwinski  |  Comment (0)

Who is ASHRAE and how can they help data center mangers save energy?

The American Society of Heating, Refrigeration and Air-Conditioning (“ASHRAE”), founded in 1894, is an international organization with 51,000 persons. ASHRAE fulfills its mission of advancing heating, ventilation, air conditioning and refrigeration to serve humanity and promote a sustainable world through research, standards writing, publications and continuing education. One such publication is the “Best Practices for Datacom Facility Energy Efficiency” in which they define the recommended temperature and humidity level as measured at the inlet of datacom equipment. A valuable point to note is that the 2009 recommended upper limit temperature is 80.6 degrees F which is an increase of 3.6 degrees F over the 2004 recommendation. It is also important to note that the specific recommended range is defined more precisely on a Psychrometric chart in which each point is defined by the dry-bulb temperature and the relative humidity.

It is widely accepted that you can save energy by avoiding over cooling a data center. More on this in my next post.

James Cerwinski