博客

Smarter Data Center Infrastructures Are Critical to Business Success and Digital Transformation

Posted on June 6, 2017 by Gento

Data centers that employ smart infrastructures and dynamic infrastructure management tools experience fewer problems and security breaches, according to a recent special study conducted by global research firm IDC and sponsored in part by Raritan.   

IDC reached out to almost 400 data center professionals to gain a comprehensive look at current data center management practices.  The respondents – ranging from CTO to facilities manager – represent the views of enterprises (72.6%), service providers (22.6%) and colo providers (4.8%).   

"This special study uncovers key challenges that organizations face in managing their data centers and how these challenges are impacting the business today,” says Jennifer Cooke, IDC research director - Datacenter Management, who spearheaded the special study.  “As data centers will bear the burden of digital transformation initiatives in the coming years, addressing these challenges through investment in smarter data center resources – such as DCIM and intelligent cabinets – will be critical to success.”

Findings from “IDC's Datacenter Facilities Infrastructure Management and Operations Special Study” include:

  • Organizations that are using dynamic infrastructure management solutions experienced fewer problems with data security breaches, physical security breaches, and running out of IP addresses.
  • Use of dynamic management tools linked to fewer regulatory/compliance fines – Data centers that use a dynamic infrastructure management solution are less likely to be fined for regulatory or compliance issues than those that do not.
  • Sixty-three percent of the respondents said that they use DCIM and listed energy consumption reporting and environmental reporting among the most important DCIM features.  The top features in order of importance are: “Reporting and Analytics,”  “Real-time Reporting on Environmental Conditions,” “Energy Management” and “Real-time reporting of energy consumption.”  Although 60+ % respondents indicated that they use DCIM, many use other methods of managing infrastructure at the same time (Excel being the most common).
  • IDC believes that DCIM implementations to date have supported better inventory control, audit, and management and that the next phase of DCIM maturity will include integrations to streamline service and workflow in the data center.  When this happens, common issues such as downtime due to human error (which is consistently a top issue in data centers) could be positively impacted by DCIM adoption.
  • Converged IT architectures put greater demands on data centers.  Organizations are adopting new technology with the goal of speeding the time to deploy new applications, but according to this study, 83.9% of respondents said that the new technology required a retrofit of power infrastructure, and 29.3% of respondents said they experienced delays in deployment because they were not able to accommodate the new technology.  The very problem that organizations are trying to solve — reducing the amount of time it takes to innovate and deploy new workloads — is actually made worse because of their failure to accurately assess and plan for the power and cooling resources needed.  Overcoming this challenge will require a greater focus on more holistic capacity planning activities, which can be addressed through investment in new processes and leverage data from more intelligent infrastructure.  More than ever, IDC believes that investment in smarter data center resources is integral to delivering IT service at the speed that business needs to innovate.

“The IDC research results confirm what we hear from our customers.  Data centers best equipped to support business innovation and digital transformation are those that have real-time and complete visibility into operations by using smart infrastructures – such as our intelligent power solutions, Xerus Technology platform and Data Center Infrastructure Management Software,” says David Wood, Director of Raritan’s Power Business.

Click here to view more IDC insights on the future of smart data centers.

Other Blog Posts

The cascade effect of data center failure on businesses - why sensors are essential
Posted on November 5, 2023
人工智能的快速发展和使用力登PDU满足更高的电力需求
Posted on October 11, 2023
Data Center Report Fewer Outages, But Downtime Still Costly
Posted on September 20, 2023
Survey: Energy Usage and Staffing Shortages Challenge Data Centers
Posted on September 20, 2023
力登安全交换机(RSS):安全NIAP 4.0兼容式桌面型KVM
Posted on September 20, 2023

View all Blog Posts

力登官方微信公众号

力登官方微信公众号
cn-blogfollow

近期活动
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
力登最新新闻

重振数据中心行业—罗格朗重磅推出两款革命性的智能机架式PDU!