部落格

Physical Security and Audit-Readiness at the Rack

Posted on July 23, 2018 by Gento

As a growing volume of sensitive data increasingly floats across your cloud and virtualized infrastructure, it’s easy to think about security and compliance in non-physical terms. That’s because compliance mandates such as HIPAA, PCI, and GDPR require your organization to protect data no matter where it resides. And if an attacker breaches your environment through a phishing email or an unpatched vulnerability, there’s no telling where they can wind up as they probe laterally across your network.


Data Center Cabinet Load Balancing:  there’s a less complicated way.

Posted on March 28, 2017 by Gento

Rack PDUs in a Server Rack

Why do we load balance?

Without going into the complicated math, suffice it to say that load balancing in a 3 phase system is desirable.  The more unbalanced a system the more problems it creates.  UPS life, for one, can be affected by unbalanced systems.  Although one circuit (server cabinet) being out of balance won’t have much effect, if many or all circuits on a panel are out of balance, the main circuit supplying the breaker panel will be out of balance and this can ruin your upstream UPS.  There are also efficiency issues with unbalanced loads.

How is load balancing currently accomplished in a rack cabinet?

To balance a load in a cabinet, the loads of the equipment power supplies are spread across the 3 phases – L1/L2, L2/L3, L3/L1.  This is done by plugging the first server (or switch/router) in an outlet wired on L1/L2, the next server on L2/L3, the next on L3/L1, then start over.  The goal is to get an equal number of devices/loads on all 3 phases – or as close as possible. 

This approach can quickly turn into a cabling nightmare. Most rack PDUs are linear in their phase layout of outlets – there are only three banks of outlets, one for each phase.  For example, on a 36 outlet PDU, outlets 1 through 12 will be on L1/L2, 13 through 24 on L2/L3, and 25 through 36 on L3/L1.  If you use the above method of balancing, and start racking the devices at the bottom U position, the third device you plug in will need to reach the top third of the PDU and the last device may have to reach back to the bottom of the PDU.  In other words, a lot of crisscrossed cabling.

How do Raritan’s balance the cable and load balancing challenge?

In certain Raritan PX three-phase models the architecture gets around the cabling issue by staggering the grouping of outlets - there are at least 6 banks of outlets.  For example, outlets 1 through 6 are on L1/L2, 7 through 12 on L2/L3, 13 through 18 on L3/L1, but then we start over at L1/L2 for outlets 19 through 24. (See Illustration below)

This intelligently engineered architecture results in more reliability and easier execution.  The devices towards the top of the cabinet don’t need to be plugged in to the bottom of the PDU and devices at the bottom don’t need to be plugged in to the top.


Limited complimentary passes available for DatacenterDynamics San Francisco Show

Posted on June 28, 2013 by Gento

Raritan has a limited number of complimentary passes valued at $495.  Contact Dorothy Ochs at Dorothy.Ochs@Raritan .com or (732) 764-8886 x1220. 

Don’t miss our presentation titled “Deploying High Power at the Rack – How to Determine and Design for Peak Power Demand.”  Time: 2:10 - 2:50 PM, Location: Hall 3.  We will be raffling an Up by Jawbone at this session.

And don’t forget to visit our booth to see the latest power management and DCIM solutions.  We are also raffling a GoPro camera at the booth.  Hope you can join us.


Benchmark Your Data Center - May 23 in Atlanta

Posted on May 9, 2013 by Gento

Benchmarking your Data Center  

Key Note Speaker: EDI, Ltd.‘s Jeremy Gilbertson, CTS, RCDD  

Topics Covered:
- Why Most Data Center Projects Fail Before They Begin. The importance of benchmarking and accurate statement of requirements
-  State of the Industry – Data Centers: Interesting, unique goings-on in the data center industry  

Jeremy Gilbertson, CTS, RCDD is Vice President of EDI, Ltd.‘s Data Center Practice and is responsible for overall strategic direction, management, and project delivery for the practice. Jeremy’s expertise involves helping enterprise, third-party provider, healthcare, and higher-education clients understand the current state of their data centers and develop phased strategies that address business requirements, risk profile, and budget. 

Join us for an afternoon of leading edge Data Center discussions and real world case studies ranging from design through intelligent infrastructure management followed by a tasting of best brews and appetizers. 

REGISTER HERE
Space is limited.

When:Thursday, May 23rd from 12:00pm-5:00pm
Where: Gordon Biersch Brewery - Buckhead location
3242 Peachtree Road N Atlanta GA 30305
Agenda

Case Studies on Tap:
- Raritan: Deploying High Power at the Rack
- Fluke Networks: Ensuring Performance of Critical, High Bandwidth Fiber Links
- Global Power Technologies: Power Monitoring Systems Enhance the Commissioning Process for a Fully Integrated Facility
- Vigilent Corporation: Too Cool - Changing the Game in Data Center Cooling    

About EDI, Ltd.  EDI, Ltd. is a leading healthcare IT consulting and design firm specializing in medical communication technologies, information systems infrastructure, security, audio-visual systems, and data center.   

Attendees will be entered into a drawing for a Kindle Fire! 

REGISTER HERE
Space is limited.


Visit Us at the Uptime Symposium – Learn and Maybe Even Win

Posted on May 2, 2013 by Gento

Stop by our booth (#219) and see why we were recently named to CRN’s 2013 Data Center 100 list

Get a $600 registration discount on us—Use code RARITANCLIENT Register Now -

Raritan is a proven innovator of power management, DCIM software, KVM and serial solutions for data centers of all sizes. Stop by our booth for live demos to learn about some of our latest solutions, which inlcude:

- SecureLock™ - Never worry about your cables accidentally unplugging
- Wi-Fi Kit - Keep your iPDUs connected with savings, security and easy implementationd
- cTrack - This new release of dcTrack®  3.0 DCIM software provides additional capabilities to make it easier for data center professionals to obtain information on their data center infrastructures

Stop by and be entered into a drawing for an iPad mini.


Page 1 of 3 pages  1 2 3 > 

訂閱

近期活動

Data Cloud India
February 5-6, 2020  •  Mumbai, India
Industrial Automation
April 24, 2020  •  Tainan, Taiwan
DigiTimes Data Center Forum Taipei
May 8, 2020  •  Taipei, Taiwan
Cloud & Data Center Convention (Wmedia)
May 14, 2020  •  Manila, Philippines
Industrial Automation
May 14, 2020  •  Taipei, Taiwan

View all Events

Raritan最新新聞

Raritan Introduces Economical New Generation KVM-Over-IP Switch and Serial Access for SMBs
Posted on March 16, 2020
Extended IT rack power mapping possibilities with Raritan’s locking solution
Posted on October 23, 2019
Raritan Ranked as the Global Leader in KVM-over-IP Switches
Posted on October 21, 2019
Raritan’s New KVM-over-IP User Station Brings 4K Performance and Productivity to Remote Equipment Access
Posted on September 18, 2019
Raritan’s New 4K Ultra HD KVM-over-IP Switch Wins Best of Show Award at NAB
Posted on May 22, 2019

View all news