Overview
This extension enables ClickOnce apps in Google Chrome.
This extension adds support for launching ClickOnce applications from Google Chrome. It is needed for launching the Cegid Peoplenet product although it can be used with any ClickOnce-based application. Changelog: Version 1.4 [ENH] Change the name of the extension due to rebranding (former name: Meta4 ClickOnce Launcher) Version 1.3 [FIX] Avoid the .NET Framework 2.0/3.5 requirement that might appears in some environments. Therefore, in this case, installation issues with the helper executable will be solved. [ENH] Branding changes Version 1.2 [FIX] Solves download issues with the helper executable in Chrome 55 and upper. Version 1.1 [FIX] Tab kept on loading state after to launch a ClickOnce app. [FIX] Some URLs which contains 'application' was processed incorrectly. [FIX] In rare situations the Microsoft launcher process used by the extension was kept in memory. [ENH] More info in the install page. Version 1.0 First version
Luke MastenJan 20, 2023
initiates unwanted downloads that chrome also doesn't trust. i came back to my PC with an uncompleted download from 4AM
JJ TanSep 27, 2022
doesn't work at all. this extension is long overdue without newer releases
James CookSep 21, 2022
Doesnt work. Waste of time! Chrome Version 105.0.5195.127 (
Details
- Version1.4
- UpdatedJanuary 31, 2023
- Offered byCegid Spain S.A.
- Size52.38KiB
- LanguagesEnglish
- DeveloperCegid
Cegid Spain S.A.
Centro Empresarial Europa Rozabella 8 Las Rozas, Madrid 28290 ESEmail
meta4development@gmail.com - TraderThis developer has identified itself as a trader per the definition from the European Union.
Privacy
This developer declares that your data is
- Not being sold to third parties, outside of the approved use cases
- Not being used or transferred for purposes that are unrelated to the item's core functionality
- Not being used or transferred to determine creditworthiness or for lending purposes