Cat5 KVM, KVM-over-IP, Remote Network Management, Power Management (PDU), Server Management and Network Monitoring Solutions
| United States |
Home > Resources > Screenshots > Dominion PX
Email
E-MAIL

PRINT

Dominion PX Screenshots

Outlets Display

Outlets Display

Turn individual outlets OFF and ON and monitor the individual outlets and the rack PDU overall. Each outlet features an icon whose color and flashing status indicates the status of the outlet.

Outlet Details

Outlet Details

Displays the current, voltage and power values and status of a specific outlet in real time, and allows the user to power on, off and power cycle the outlet.

Event Log Settings Window

Event Log Settings Window

Allows users to configure event logging, including selecting the desired events and entering the e-mail address for notifications or other standards-based methods for storing events. For example, you can configure Dominion PX to alert someone via e-mail when critical rack temperature thresholds are achieved or PDU power consumption is nearing critical and will soon trip a circuit if not attended to. You can also configure it to simply store the event in an NFS log or forward to an SNMP enterprise management system.

Outlet Setup Window

Outlet Setup Window

Allows users to give each outlet a name to help identify the connected devices and to set non-critical and critical thresholds. For example, if the non-critical threshold for outlet #2 is set at 3.0 amps, and the device plugged into outlet #2 draws 3.4 amps, the LED for outlet #2 will flash red because the actual current draw is greater than the threshold. And, an e-mail alert would be sent if desired.

Certificate Signing Request Window

Certificate Signing Request Window

Allows administrators to manage Secure Sockets Layer (SSL) server certificates to ensure maximum security for controlling power in the data center, allowing only authorized users to remotely recycle power to equipment in local or remote data centers.

Network Settings Window

Network Settings Window

Network connectivity configurations can change using the Network Settings Window and includes support for user customizable port settings.

Alert Configuration Window

Alert Configuration Window

Allows users to set event policies, for example, configure Dominion PX to send an alert if a particular outlet’s current draw exceeds the critical threshold set by using the Outlet Setup Window.

User/Group System Permissions Window

User/Group System Permissions Window

Allows administrators to set up system-level access and permissions for individual users and user groups with granular access control permissions on a user or group level.

User/Group Outlet Permissions Window

User/Group Outlet Permissions Window

Allows administrators to set up outlet-level access and permissions for individual user and user groups. This provides the ability to segregate outlets to specific types of users or groups of users within departments. For example, Cisco admins only have access to control or switch outlets that Cisco equipment is plugged into.

Unit Setup Window

Unit Setup Window

Allows administrators to custom configure time delays for outlet on and outlet sequencing upon turning on the Dominion PX for the first time or when a circuit fails.  This is very important to prevent circuit failure issues related to in-rush current.

Authentication Settings Window

Authentication Settings Window

Allows administrators to configure local user authentication or leverage an existing enterprise directory service like LDAP or RADIUS.

User/Group Management Window

User/Group Management Window

This window allows administrators to set up users including passwords and assignment to groups. Dominion PX supports strong passwords to maximize security.

HOW TO BUY

To learn more about our solutions, or to buy now, please choose from the following:

Call: (800) 724-8090