Cat5 KVM, KVM-over-IP, Remote Network Management, Power Management (PDU), Server Management and Network Monitoring Solutions
    
| United States |
Email
E-MAIL

PRINT

Cat5 Reach

Cat5 Reach

OVERVIEW

 

Cat5 Reach enables you to remotely access a single PC or multiple servers connected to a KVM switch. The remote user console (keyboard, monitor, and mouse) can be up to 1,000 feet away from the PC or KVM switch. Cat5 Reach allows you to:

    * Operate a PC from wherever you want to be.
    * Keep your PC in a clean, secure environment.
    * Protect the PC, applications and valuable data.
    * Add a local user console, in addition to the remote user console.
    * Control all servers connected to a KVM switch remotely.

View the technical specifications for Cat5 Reach

Cat5 Reach is easy to install and easy to use. Each Cat5 Reach model is packaged as a kit that includes a transmitter and receiver pair for use with your Enhanced Cat5 UTP cable. Just plug a keyboard, video and mouse into the receiver and operate. Automatic Video Tuning (AVT) adjusts video quality automatically, so no manual adjustments are needed.

Cat5 Reach is available in the following models:

UPCED (for PC), USNED (for Sun), USBED (for USB):
Allows location of a user console (keyboard, monitor, mouse) up to 1,000 feet away from a PC, or CompuSwitch, MasterConsole II or other KVM switch.

UPCEDF (for MX4)
Allows location of a user console up to 1,000 feet from a MasterConsole MX4, CompuSwitch or other KVM switch.

UPCEDE (for MX4)
Allows cascading of MasterConsole MX4 units up to 1,000 feet away from another MX4.

UPCEDU (for PC), USNEDU (For Sun), USBEDU (for USB)
Allows location of a PC, Sun or USB PC up to 1,000 feet away from any Raritan or other KVM switch.

AUPUSBC (for USB)
Allows connection of one (1) USB PC — with KVM ports for local access.

 

BENEFITS

 

Features and innovations that deliver what you demand.

  • Automatic Video Tuning (AVT) in URKVMG receiver unit adjusts video quality automatically.
  • High quality video to 1280 x 1024 resolution at 650 feet and 1024 x 768 resolution at 1,000 feet (305 meters).
  • Support of Macs, Suns or ASCII devices with Raritan's converters.
  • Local user console connection in addition to the remote user console for additional convenience.

FAQ

 


How can I get access to more servers if I have already connected computers to all my KVM switch channels?
Cascade any KVM switch (except SwitchMan) to expand the capacity.


What is the distance between cascaded units?
Two feet to 30 feet with Raritan coaxial cables. By using Cat5 Reach, cascaded switches can be up to 1,000 feet apart. Or, by using FiberReach II, cascaded switches can be up to 6,600 feet apart. Additionally, user consoles and PCs can be 1,000 or 6,600 feet from the KVM switch with Cat5 Reach or FiberReach II.


What will happen if I use more than 1,000 feet of Category 5 cable on my Cat5 Reach?
The Cat5 Reach is designed to operate at maximum performance up to 1,000 feet. If you use a Cat5 cable longer than 1,000 feet, you may see a degradation of the video quality and/or a loss of keyboard or mouse operation. You will not harm the Cat5 Reach components with a longer cable.


I have some computers located more than 30 feet away from my KVM switch. Can I connect these computers to my KVM switch?
Yes. To locate computers or cascaded KVM switches at distances greater than 30 feet from the KVM switch, use Raritan's Cat5 Reach with standard Category 5 UTP cable (up to 1,000 feet) or FiberReach II with fiber optic cable (up to 6,600 feet). Call Raritan Sales for more assistance.


I need to relocate one of the servers, but the current cable kit is not long enough. Is there any way to extend the distance?
Yes, use Raritan's Cat5 Reach with standard Category 5 UTP cable (up to 1,000 feet) or FiberReach II with fiber optic cable (up to 6,600 feet). Call Raritan Sales for more assistance.


I intend to place my switch in a rack or enclosed cabinet with the servers. Is there a simple way to switch and operate the servers from my desk without going to the rack?
Yes. Use our keyboard, monitor, mouse extension cable, up to 35 feet, and operate using hot-key commands and on-screen menus. To locate user consoles at distances greater than 35 feet from the KVM switch, use Raritan's Cat5 Reach with standard Category 5 UTP cable (up to 1,000 feet) or FiberReach II with fiber optic cable (up to 6,600 feet). Call Raritan Sales for more assistance.

ORDERING INFO

Skip Navigation Links.
Expand <div runat='server' id ='divSectionNode' class ='SectionNode' visible ='true'>KVM Extenders</div>
KVM Extenders
Expand <div runat='server' id ='divSectionNode' class ='SectionNode' visible ='true'>Accessories</div>
Accessories

Poll

When thinking about how you run/operate your data center today, what area do you want to improve first?

Get an accurate view of what data center assets you have and where they are located
Implement a data center change management process
Improve data center capacity planning and utilization
Make my data center green and more efficient

What's New?

Dominion KX II - The world's Best KVM-over-IP switch now supports IBM, HP and Dell blade servers!

LEARN MORE

You can access your virtual servers and the physical infrastructure (blade servers, rack servers, networking devices) all from a single ubiquitous interface.

Raritan solutions provide consolidated access and centralized security for your entire IT infrastructure. 

Read More

HOW TO BUY