The Raritan Blog

Raritan PX Intelligent PDUs: Making your Data Center Power More Reliable

Nicolas Sagnes
September 6, 2017

The core of any successful data center management team is uptime and service availability. Data centers need infrastructure hardware that can guarantee the highest levels of service continuity throughout their entire life cycle. This is imperative as the cost of a power outage is on the rise, according to the latest data center report that “the average total cost per minute of an unplanned outage increased from $5,617 in 2010 to $8,851 to 2016”. It’s critical for data center managers to put in place processes and procedures related to their infrastructure in order to prevent potential outages causing downtime. They not only need to be alerted right away when anything out of the ordinary occurs but also enable quicker recovery when the worst case happens.

Since intelligent PDUs are the closest point of contact with IT equipment, they play a pivotal part in managing these infrastructure processes and procedures. Amongst these intelligent PDUs, Raritan iPDUs are one of the most reliable devices, as they are tested and deployed within some of the world’s largest data centers. The PX iPDUs provide the most advanced features to empower concerned users by supplying reliable power to the rack while reducing downtime.

In terms of reliable power, not all features are equal. Some key elements that impact your ability to guarantee uptime are: