The Raritan Blog

Data Center Storage and Networking with the iX7 Advance Controller

Rick Gonedes
August 17, 2017

The iX7 PDU Controller was designed from the ground up to allow operators to make the most of their available resources in a way that positions them to not only meet the challenges of today but to address the demands of the future. It can be integrated into existing PX3 intelligent  PDU models with no additional costs required. At the same time, it brings those PX3 models more ports, more computing power, and the ability to execute more varied applications to help operators manage their data centers more efficiently and at lower costs than ever before.

Complete with a future-proof design architecture, the iX7 is a PDU controller that is built to stand the test of time in more ways than one.