部落格

Demand for Faster, Denser Data Center Networking

Posted on February 8, 2018 by Gento

As business innovates, data centers are feeling a crunch. Their customers demand speed and density, no longer satisfied with what once seemed cutting-edge. Find out how data network center designs are changing at every level to focus on speed and density.

Businesses Continue to Invest in Data Centers

For now, it seems businesses are content to invest in data centers as they explore the cloud. A 31 percent of responders to a recent survey from Network Computers Report plan to invest half, or more, of their IT budgets in data center facilities, operations, or hardware in 2018. Companies plan to spend the most amount of money on servers, while virtualization and public cloud services are also top priorities.  

Rich Media Behind Demand for Faster Connection Speeds 

Where 10 gigabit Ethernet connections used to be large enough to accommodate both inter-center (east-west) and intra-center (north-south) traffic, this is no longer the case. From big data to rich media, customers are simply flooding the data center with larger packets of data than the Ethernet connections can accommodate.

In some data centers, connections have increased tenfold to 100 gigabit Ethernet -- and not merely at chokepoints, but throughout the data center. 

Some enterprise data centers are exploring Ethernet alternatives, too, be it dedicated wavelengths or robust dark fiber in their quest to keep pace with changing demands for speed. 

Flat Design is Falling Out of Favor 

From the original flat design, networks grew tiered, then flat, and then tiered into the leaf-spine shape that has become the current standard, offering a balance between flat and resilient. The flatter the network, the less an individual data packet has to travel to pass through the data center. 

Recently, deep design is coming back into favor. We're starting to see a resurgence of the three-tier structure where intermediate points connect branch nodes to one another, to the data center, and to the internet. In some data centers, there's more complex networking due to WAN-cloud exchanges, which leverage the benefits of the cloud with the reliability and security of the data center.

WAN-cloud exchanges offer a virtual alternative to physical infrastructure management for these connections, relying on exchange routers for connectivity rather than direct-to-cloud routers. WAN-cloud exchanges serve as connectivity hubs between many different cloud service providers and enterprises.

Since they're virtual, data centers can set up many more of these WAN connections than they can direct connections. What's more, WAN-cloud exchanges are easy to set up, secure, and agile. It takes minutes to spin up a virtual direct connection at the moment of need. With WAN-cloud exchanges, data centers are limited only by their imagination in their options for link connectivity.

Cloud Resources Demand Fast Connectivity

The widespread adoption of cloud resources also plays a role in the push for faster data centers. Customers need speed to connect cloud resources to the data center's applications or to accommodate their onsite cloud users, and data centers need cloud resources to stay cost-effective.

Data centers have started connecting at the edge to cloud providers' networks through colocation facilities, either physically or through a point of presence, increasing capacity while decreasing lag time. Technologies like Direct Connect (from Amazon Web Services) or ExpressRoute (Microsoft Azure) are driving this edge connectivity. This sort of edge computing is projected to grow, and bring with it major changes to the flow of information through data centers. 

Staying on top of trends in the data center can help your company make better decisions, provide better service to customers, and remain future ready. How will you prepare for what 2018 brings? To learn about how the latest innovations in power distribution are meeting the demand for increased speed with a Standard Gigabit Ethernet click here.  

Other Blog Posts

從資料中心失效對企業帶來的骨牌效應──探討感測器的重要性
Posted on November 5, 2023
更高規格的電源要求加速AI市場成長與Raritan PDU的採用
Posted on October 11, 2023
資料中心服務中斷次數減少,但停機的代價仍舊可觀
Posted on September 20, 2023
意見調查:資料中心面臨能源使用與人力短缺困境
Posted on September 20, 2023
Raritan安全切換器:相容於Secure NIAP 4.0的桌上型KVM
Posted on September 20, 2023

View all Blog Posts

訂閱

近期活動
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
Raritan最新新聞

Legrand 使用兩大創新智慧型機架 PDU 重新活化資料中心產業
Posted on May 1, 2023
Exclusive interview丨How does Huizhou upgrade its manufacturing industry?
Posted on December 2, 2021
Raritan 發表 MasterConsole® 數位雙電腦切換器
Posted on February 18, 2021
Legrand Data, Power and Control Division Announced as Finalist in Six Categories at DCS Awards 2020
Posted on November 9, 2020
Raritan 新款智慧機櫃控制器 (SRC) 可智慧管理資料中心與關鍵任務設施的環境與安全性資訊
Posted on November 9, 2020

View all news