博客

Understanding Overload Protection in Raritan’s Rack Transfer Switch

Posted on February 16, 2016 by Gento  |  Comment (0)

This past week, we opened our mailbag and found the following customer email:

Dear Raritan team,

We mostly love the 16A rated rack transfer switch so far! The physical design made it easy to connect power feeds from the back of the cabinet. The outlet-level metering and switching let us power off development servers no one was using on weeknights and weekends.  But, here’s one thing that wasn’t so great:

We recently experienced a total device failure.  We weren’t sure what it was at first, but quickly realized it was a blown fuse from both the web interface and indicator lamp/alarm on the unit. Once we replaced the fuse the unit continued operating just fine.  But, why is it there in the first place? And why not have a circuit breaker instead of a fuse?

Tl;dr What is the purpose of the fuses located on the inlet side of Raritan’s rack transfer switch and why not have a circuit breaker instead? 

Those are great questions.  So first, let’s address the question of why the fuse is there in the first place.  The purpose of the fuse (rated at 32A) in the 16A rated transfer switch is to protect the switching circuitry in case of an IT device power supply failure that results in a short circuit (fast, high current spike).  This particular type of fuse is what’s called a fast-blow fuse.  It is commonly used in electrical equipment where an overload current can damage sensitive circuitry.

But, don’t confuse this with normal circuit overcurrent protection which is already provided by the facility’s circuit breaker.  For example, if you were to load the transfer switch and exceed 16A, the facility’s breaker would trip but the fast-blow fuse would remain intact. 

On the other hand, if say, the server plugged into outlet number one on the transfer switch were to experience a power supply failure (resulting in a short circuit and high current load spike), the fast-blow fuse on the inlet side would quickly melt and break to protect the rest of the unit from being damaged or even going up in flames!

Now, on to the second question: why fuses are used for overload protection instead of circuit breakers.  Fuses are used in place of circuit breakers for two specific reasons.  The first reason is that fuses have a more exact tripping point and faster response time than most circuit breakers. 

The second reason is that most circuit breakers are designed to trip a finite amount of times.  And, although it’s easier to reset a breaker than it is to replace a fuse, once the breaker needs to be replaced, there’d be no way to do it out in the field because the breaker would be soldered on to the switch.

So any way that you slice it, you’re better off paying $15 for a pack of two dozen fast blow fuses, than you would be if you had to replace the entire transfer switch or ship it back to Raritan for repairs.

Other transfer switch solutions in the market today do not offer field serviceable fuse protection.  So, when the IT device power supply fails and a short circuit occurs, the device switching circuitry will also fail and the entire unit will need to be ripped out of the rack and replaced.

Side note: For our 30/32A transfer switch configurations, the unit has both fuses and circuit breakers.  The circuit breakers are required to protect the branch circuits in the same way they are used on a rack PDU (required for any PDU greater than 20A rated).  The fuse is rated higher than the facility circuit breaker so it can protect the switching circuitry from high current spikes caused by IT device power supply failure.  


Learn more about what sets Raritan’s rack transfer switch apart, or contact our sales department for a no-strings-attached price quote. 




Other Blog Posts

Weak Links in Security Part 1: Configuration Is the Biggest Security Threat
Posted on March 28, 2018
The Challenges You Face with IoT and How To Overcome Them
Posted on March 15, 2018
Virtualization and its Challenges for Server Rooms
Posted on March 6, 2018
IoT is Taking Over, Secure and Prepare Yourself
Posted on February 23, 2018
What Money Pitfalls to Avoid When Building a Data Center
Posted on February 16, 2018

View all Blog Posts

力登官方微信公众号

力登官方微信公众号
cn-blogfollow

近期活动

Cisco Live 2018
March 6-9, 2018  •  Melbourne, Australia
DataCloud Asia 2018
March 22, 2018  •  Singapore
DCD Indonesia
Apr 5, 2018  •  Jakarta
Data Centre World Hong Kong
May 16 – 17, 2018  •  Hong Kong
CDCC China
May, June, July, Nov 2018  •  Wuhan, Hangzhou, Chengdu, Beijing

View all Events

力登最新新闻

Finding Weak Links in Your Security Policy and How to Safeguard Data Centers Will Be Addressed by Raritan Speaker at AFCOM Conference
Posted on March 8, 2018
Raritan Introduces Secure Switch for KVM Access to Government and Military Computers
Posted on March 6, 2018
Ashley Fox of Raritan Inc. Recognized as 2018 CRN Channel Chief
Posted on February 27, 2018
Packet, Myriad Supply, Raritan, and Data Center Knowledge to Participate in ‘Managing the Edge’ Webinar
Posted on November 12, 2017
Raritan Employees Support Green Community Projects
Posted on November 8, 2017

View all news