博客

Preventing Human Error in a Data Center

Posted on October 30, 2017 by Gento

Many people don't realize that the most significant cause of data center downtime, to the tune of an incredible 70% by most estimates, actually has to do with your employees, more specifically, human error. It's a very serious problem that will only get worse if not corrected upfront, but luckily there are a few key steps that you can start taking today to help mitigate risk from these types of issues moving forward. 

The Myth of "Malicious Intentions"

The vast majority of the time, human error has absolutely nothing to do with a person's "malicious intentions" but is the product of someone being in the "wrong place at the wrong time." Think about it - data centers, in particular, are highly specialized environments, filled with room after room of sensitive (read: fragile) equipment. All it takes is one person getting in a situation they're not equipped to handle, making a choice perhaps they think will help the team but in reality, it’s the wrong decision and next thing you know, you’re looking at a major issue.

Combatting Human Error

Human error is not something that can ever fully be eradicated.  We're all human beings and humans make mistakes. It is, however, something that you can plan for.

Color-coded power cord plugs and plug inserts, for example, are a perfect visual way to help quickly identify which resources are essential and which ones are less important. Even by someone who isn't necessarily familiar with the equipment, they are still able to recognize the proper importance.

A device that has been connected with a RED power cord, for example, might be one that is absolutely mission-critical and should never, under any circumstances, be unplugged. Any equipment that CAN be unplugged with management confirmation, on the other hand, might be connected with a YELLOW plug. GREEN power cords might be used to identify assets that are not mission-critical and therefore can be unplugged temporarily on an as-needed basis.

This is just one example of a system that you may implement and stick with, along with mandatory training for all employees, regardless of job title, to help eliminate human error. These actions will go a long way towards preventing employees who make an “educated guess” that, unfortunately, turns out to be wrong, thus taking some of your assets offline resulting in an unforeseen outage.

Another perfect opportunity to mitigate risk from human error would involve utilizing rack PDU locking power cords and outlets. Even going beyond human error, IEC outlets can oftentimes fail to hold plugs as securely as employees and data center managers would like. All it takes is one person who doesn't triple check a plug to make it secure, and you're a few hours away from an accidental disconnection.

With Raritan’s SecureLock power cords and outlets, however, this isn't something you would need to worry about anymore. All of Raritan's PX intelligent rack power distribution units are equipped with SecureLock outlets from the time of purchase, and when connected with SecureLock power cords it prevents cables from becoming accidentally unplugged, ensuring data center managers a peace of mind.

Another important area to focus on is physical data center security. Being able to limit access to only authorized personnel in a data center goes a long way towards reducing conditions where human error can take effect WITHOUT impacting the mission-critical functions of the rest of your organization. One simple solution that adds a layer of physical security to the cabinet is intelligent door locks. Raritan offers intelligent door locks called the SmartLock System which provides users an easy to deploy, economical, networked door locking solution for all types of data center enclosures. The optional USB webcam allows for even more security in highly sensitive environments with proximity sensors, which provides real-time images and video to be viewed remotely. 

These are just a small sample of the different methods of preventing human error. These steps combined with employee education, process and procedure go a long way towards greatly reducing the risk from the number one cause of data center unplanned outages today, human error.

Other Blog Posts

The cascade effect of data center failure on businesses - why sensors are essential
Posted on November 5, 2023
人工智能的快速发展和使用力登PDU满足更高的电力需求
Posted on October 11, 2023
Data Center Report Fewer Outages, But Downtime Still Costly
Posted on September 20, 2023
Survey: Energy Usage and Staffing Shortages Challenge Data Centers
Posted on September 20, 2023
力登安全交换机(RSS):安全NIAP 4.0兼容式桌面型KVM
Posted on September 20, 2023

View all Blog Posts

力登官方微信公众号

力登官方微信公众号
cn-blogfollow

近期活动

New Zealand Cloud & Datacenter Convention 2022
3 November 2022, 9am – 4pm  •  Grand Millennium Hotel, Auckland, New Zealand
Data Centre World Singapore
12th – 13th Oct 2022
Korea Cloud & Datacenter Convention 2022
6th Oct 2022
Philippines Cloud & Datacenter Convention 2022
4th Aug 2022
JANOG50 Meeting Hokkaido
3th – 15th July 2022

View all Events

力登最新新闻

重振数据中心行业—罗格朗重磅推出两款革命性的智能机架式PDU!
Posted on May 1, 2023
独家专访丨惠州如何升级制造业?法资企业CEO提了个建议
Posted on December 2, 2021
力登公司推出MasterConsole®数字双显示器KVM切换器
Posted on February 18, 2021
Legrand Data, Power and Control Division Announced as Finalist in Six Categories at DCS Awards 2020
Posted on November 9, 2020
力登公司(Raritan)推出新型智慧型机架控制器(SRC),用于智能地管理数据中心和关键基础设施中的环境和安全信息
Posted on November 9, 2020

View all news