主页 » 博客
Posted on August 24, 2020 by Gento
虽然三相pdu提供了更高的功率容量,但它们确实需要在服务器部署之前进行更好的规划。PDU三相中的一个或两个相位的电力消耗不平衡会产生“搁置容量”,从而增加电力的浪费。此外,这种情况可能导致上游链路出现连锁故障。PX3 pdu可以主动监控相位之间的平衡情况,如果配置正确,可以在相位不平衡超过某个阈值时向您或您的管理团队发出警报。作为一个最佳实践,尽可能平衡所有三个相位的电力消耗是非常重要的,这可以尽量减少意外电力中断和浪费。
Posted on August 24, 2020 by Gento
Raritan's PX3 PDUs monitor a variety of electrical and environmental parameters. You can receive alerts on anything that gets monitored – inlet data, outlet data, circuit breaker status, unbalanced loads, and power factor, to name a few. To configure and receive alerts successfully, you need to ensure the following actions have been completed:
1. Configure Alert Delivery Mechanism – how to set up and receive your alerts: SNMP and/or SMTP.
a. If you prefer your alerts to be sent to an SNMP manager tool, you need to enable: Device Settings > SNMP > Enable SNMP Notifications
It is important to note that this setting is different from the SNMP Agent setting. You won't be receiving SNMP alerts even if you have enabled SNMP v1/ v2c if you don't explicitly enable SNMP Notifications.
Posted on June 23, 2020 by Gento
新冠疫情持续不断,企业该如何保持员工自身的安全的同时,又能让业务继续照常运作?在力登关于IT设备远程管理的博客中或许能找到答案。文中所强调的网络连接KVM交换机所带来的种种优势很详细的阐明了这一点。尽管目前来看,最糟糕的情况似乎已经过去,封锁限制正在慢慢放松,但是疫情是否还会“卷土重来”呢?这一点不得而知。因此,企业员工很大可能还是需要借助远程工具,居家办公或者异地工作。
在购买远程访问管理解决方案时,本文提供了8个实用贴士供参考,确保实现您的业务目标,同时对公司现有的资源保持密切关注,将投资利益最大化。
Posted on June 15, 2020 by Gento
新冠疫情的爆发,无疑是一场不断演变的全球公共卫生和经济危机。作为公司和企业,必须在保证业务系统正常运行的同时,保证员工的安全和健康。许多员工不得不居家办公。从全球整体情况来看,最严重的时期似乎已经过去,但疾病控制中心(CDC)警告说,秋冬季节可能会出现“第二波”疫情。在这种不确定的环境中,远程管理具有巨大的优势。
Posted on April 2, 2020 by Gento
Looking for an economical KVM solution? This blog discusses features included in the new Dominion LX II, and why it would be beneficial for you to trade up from the original Dominion LX.
The new Dominion LX II from Raritan is the latest in a line of products designed with the small to midsize business IP KVM switch user in mind. Our new unit is designed to provide economical, Java-free, BIOS-level remote access to between 8 and 16 servers as well as virtual media. The new Dominion also supports connections up to 15 frames-per-second at a resolution up to 1080p and 1200p. With six different options available, the next generation LX II is poised to become the leading SMB IP KVM switch on the market today.